Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
XLP Deep Sleep Mode Slide 21
Waking up from Deep Sleep causes a Power-On Reset, which in turn, resets most registers back to their POR default values. However, immediately applying these default settings could be undesirable in a Deep Sleep application, so a special Deep Sleep feature prevents certain register changes from being applied during start-up. Without this feature, I/O pins would all revert to being tri-stated and the RTCC would be disabled immediately on wake-up. The end result would be losing track of time and losing control over external circuitry. Instead, application firmware has a chance after wake-up to initialize values other than the power-on defaults. Afterwards, firmware will manually clear the special Deep Sleep RELEASE state bit to allow register values to actively drive the hardware once again. At this point, application-specific tasks can be carried out, such as reading new data and outputting resulting data.
PTM פורסם ב: