Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
XLP Deep Sleep Mode Slide 25
The biggest difference between the parts shown here is the core voltage regulator. The PIC24F16KA102 does not use a core voltage regulator, the entire device runs at full VDD voltage. In contrast, the PIC18F46J50/11 and PIC24FJ64GA104 use a separate core voltage, lowering power use of the processor core logic. Deep Sleep mode on these devices turns off the processor core by disabling the internal core voltage regulator. For PIC18, the LF variants of these devices lack the internal core voltage regulator; consequently, Deep Sleep mode is not available on LF parts. For the PIC24, the voltage regulator enable/disable pin must be enabled for Deep Sleep Mode.
PTM פורסם ב: