Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
XLP Deep Sleep Mode Slide 11
The most common wake-up sources available for Deep Sleep include Interrupt 0, the DSWDT, an RTCC alarm, and the ULPWU. MCLR Reset can also be used as a wake-up source. However, I/O pin states will be lost upon wake-up, instead of waiting for application firmware to clear the Deep Sleep “RELEASE” bit. A power off/power on sequence will also “wake” a device from Deep Sleep, but this will behave exactly like a traditional Power-On Reset. Data stored in special Deep Sleep registers will not be retained over a full power off/on cycle, since VDD voltage is required to maintain these Deep Sleep registers. Like MCLR Reset, power off/power on cycling will not retain I/O pin states.
PTM פורסם ב: