Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
XLP Deep Sleep Mode Slide 20
Next, firmware can check the Deep Sleep wake-up status flag to see if it is powering on for the first time or if the device is coming out of Deep Sleep. If coming out of Deep Sleep, firmware can read data from the Deep Sleep registers to determine which wake-up source was triggered and restore application context.
PTM פורסם ב: