Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Product List
XLP Deep Sleep Mode Slide 13
The DSWDT provides another wake-up source for Deep Sleep. It is a separate module specific to Deep Sleep that requires a clock source to keep track of how long to stay in Deep Sleep. Two options are available: an internal low-power RC oscillator or an external secondary oscillator. The DSWDT should always be run from the internal RC oscillator if robustness is needed, allowing an application to wake up even if a crystal failure has occurred. Configuration bits specify how long the device should stay in Deep Sleep before timing out and waking the device. Sixteen different timeout settings are available. If more granularity is needed, a RTCC alarm should be used instead.
PTM פורסם ב: