Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
your way graph
If an existing component needs to be replaced for better performance but requires the same footprint, then the BISS transistor is the answer. In this example, the mature BCP54 transistor and the BISS PBSS4540Z transistor share the same footprint, yet the benefits of using the BISS transistor increases the power capabilities from 1 amp to 5 amps. With each new generation of Nexperia BISS transistor development, the VCE saturation has been lowered significantly compared to the previous generation. From Generation 1 to Generation 3, there has been a 57% reduction in VCE saturation as seen in the graph.
PTM פורסם ב: