Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
your way ir
If the solution is to generate less heat under the same electrical conditions while maintaining the same footprint, then BISS is the answer. In this example, the BISS transistor has a power dissipation of 1.34 watts, whereas the general purpose transistor can only dissipate .65 watts. This is because a BISS transistor die assembled in the same package as its conventional predecessor dissipates less heat during operation. The actual power dissipation of a BISS transistor is reduced by 65% compared to a conventional transistor. Thus, a BISS transistor, using new mesh-emitter technology, can be selected to avoid hot spots on the printed circuit board, as demonstrated in these thermal images.
PTM פורסם ב: