Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Product List
your way zoom
Finally, if a smaller footprint and better performance is needed, then BISS is the answer. By using the 3rd Generation BISS transistors, both reduction in board space and further improvement of performance can be attained. Comparing the PBSS302ND to a BCP54, the 3rd Generation BISS allows a greater DC current rating – 4 amps versus the general purpose 1 amp rating, and lower power dissipation. The 3rd Generation BISS in an SOT457 requires 78% less board space.
PTM פורסם ב: