Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
iMX-Slide12

There are three accessory boards available, in addition to the EVK, that can help to further reduce the effort of some specific designs. The MIPI to HDMI converter allows one extra HDMI monitor to be connected in the EVK MIPI-DSI port. This is useful for applications with dual monitors showing different content. The OLED Display board allows the implementation of a local display interface via the MIPI-DSI connection. The camera board attaches to the MIPI-CSI connector in the EVK, allowing the processing of images and video. This is helpful, for example, in a face recognition application.

PTM פורסם ב: