Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
iMX-Slide9

Several segments drive the adoption of the i.MX 8M both in consumer and industrial applications. Portable industrial devices like Imaging and Scanning use high processing and low power. Also important are the product longevity and industrial qualification. Human Machine Interfaces in industrial applications are getting more sophisticated and intuitive to the operators. Machine Vision, with multiple cameras, require the support of a capable graphic processing unit and the NEON acceleration engine to keep up with the processing demand. The market is experiencing a fast adoption of vision systems. In the Building Automation and Smart Home applications, user interfaces are also getting more sophisticated. The systems are smarter using cloud-based knowledge and local processing provides fast and accurate responses.

PTM פורסם ב: