Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Product List
MEMS Flow Sensors Slide 11

The Omron MEMS flow sensors are able to function properly with the gases listed here. Differing gases have different densities which will require the flow sensors to be calibrated specifically for each gas. Non-compatible gases include hydrogen (H2) because it is very light, explosive (special equipment required for calibration), and difficult to control leakage. Helium is also potentially a non-compatible gas since it is also very light and leakage could be problematic.

PTM פורסם ב: