Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Product List
MEMS Flow Sensors Slide 13

This slide shows a bypass set-up of flow measurement using an orifice in the main channel flow path. The orifice restricts flow just enough to cause a differential pressure, proportional to flow rate, to exist on either side of it. This differential pressure causes gas to flow through the D6F-P flow sensor, again proportional to the flow rate in the main flow path, from the high pressure side of the orifice to the low pressure side. The end result is a flow sensor that can measure, with proper calibration, a wide flow rate range without being in the main flow path.

PTM פורסם ב: