Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
Snaps-Slide15

Another consideration when choosing a snap switch is the actuator force required to get the contact to switch. The FP (Free Position) is the position of the actuator when no force is being applied. The RP (Release Position) is the point at which the common contact separates from the NO contact and snaps back to the NC, when the actuator is slowly released.

PTM פורסם ב: