Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
Snaps-Slide19

The last switch consideration is whether the switch is required to be sealed against water and dust, or whether an unsealed switch will suffice. The industry standard IP rating is used to categorize the amount of seal that the switch will have. An IP54 rating is typical for a general dust seal but is not water or liquid sealed. An IP67 rated switch is common for water ingress and most outdoor applications while IP68 is pressure wash-down rated for food service industries.

PTM פורסם ב: