Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
Snaps-Slide16

The (OF) Operating Force is the typical amount of force required to get the moving contact to “snap” over to the NO contact. The point at which the contact will snap over is called the Operating Position (OP). The Operate Time is the time it takes for the snap action mechanism to achieve OP. The Release Time is the time it takes for the snap action mechanism to achieve RP. If arcing is present, then these characteristics have a significant impact on prolonging the switch contact's lifetime. One benefit of the snap switch design is that it keeps this timeframe as short as possible.

PTM פורסם ב: