Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
SP Caps Slide 18
This slide is an example of how the low ESR and low impedance of the "SP-Cap" allows it to meet the transient response of the processor with 50% to 80% less total capacitance than polymer or conventional tantalum capacitors. This can reduce component cost and reduce board space.
PTM פורסם ב: