Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
Evaluation Boards and Reference Designs

Shown here are the design tools available for development. NXP has a full 8M reference design that incorporates Rohm’s BD71837AMWV. They also have an 8M Mini EVK that is populated with the BD71847AMWV. Finally, there is an NXP EVK for the 8M Nano that uses BD71850MWV with DDR4 memory. Additionally, if the customer wants to evaluate ROHM’s PMIC separately, there is a standalone evaluation board available as well.

PTM פורסם ב: