Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Product List
BD71850MWV + i.MX 8M Nano Block Diagram

Here is the block diagram of the BD71850MWV operating with the i.MX8M Nano applications processor. As mentioned before, the only main difference in the power side is to depopulate two rails, BUCK5 and LDO4. The BD71850MWV automatically adjusts the power sequencing for the change from the i.MX8M Mini to Nano configuration.

PTM פורסם ב: