Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List Associated Content
est total clock
After understanding how to select a clock tree component based on jitter, next the engineer needs to know how to estimate the total clock tree jitter, end-to-end. The total clock tree jitter should be estimated to determine if there is sufficient system-level design margin before the clock tree is committed. A component with poor performance can compromise the whole system. Thus, understanding jitter specification of each component is an important basis. With this information the engineer can estimate the entire clock tree’s jitter. Two critical points to note: total jitter is not the sum of the MAX RMS specifications of each component and total jitter is the root of the sum of squares of each device's MAX RMS jitter, as shown in the formula here.
PTM פורסם ב: