Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Product List Associated Content
clock gen1
Clock generators are integrated circuits (ICs) that generate multiple output frequencies from a single input reference frequency. The input or reference frequency is supplied by a crystal, XO or other clock in the system. Clock generators may have other features that can be controlled by I2C or pins such as: turning on/off outputs, skewing frequencies, and adding/removing spread spectrum to frequencies to reduce noise. The perceived challenge with clock generators is system layout. Placing a crystal adjacent to its target IC is simple and cheap. Routing a clock signal from a clock generator to its target IC might not always be as easy, although it can save money. Careful design and other techniques can ensure a centralized clock source provides equal performance. Generally speaking, if four or more clocks are required designers can save money with a clock generator.
PTM פורסם ב: