Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
Automotive Grade Transistors and Discretes Slide 13

During all the phases of the diffusion of a lot, if there is incorrect control of the process in an area of the wafer, usually it will happen in the same area in all the wafers of the lot. Wafer Map Stacking analyzes the yield for the stacked X/Y position and if the yield is lower than the minimum specified for the line, the good dice in the position X/Y are also inked as rejects.

PTM פורסם ב: