Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
Automotive Grade Transistors and Discretes Slide 3

If a supplier will not ship parts with risk of failure to the customer, it is easier to reach the Zero-defect level of quality. The failure can result from a bad manufacturing process or specifically from an issue in the automotive application. To remove the parts with a risk of failure, the Automotive Electronics Council has issued some key criteria to follow when a supplier designs, qualifies, tests, and manufactures the parts in order to have a device for automotive application. A product compliant with these requirement is an automotive grade device.

PTM פורסם ב: