Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Product List
Automotive Grade Transistors and Discretes Slide 8

A PPAP can be delivered only for an automotive grade device. STMicroelectronics can not do a PPAP, even at a level one, if a device is not automotive grade. The second important point is that the PPAP contains confidential information and will only be sent if there is a nondisclosure agreement with the customer.

PTM פורסם ב: