Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Product List Associated Content
serial tera term
Another embedded feature common to all the Function Packs is the integrated Serial Line Monitor. It is helpful for a real-time observation of the progress and status of the software routines. The user can connect the development board to the PC through a PC USB port. From the device manager of the PC, the development board will be seen as a Virtual COM port. A serial terminal emulator, e.g. TeraTerm, can be opened on the PC (with the port setup setting shown here). This feature is very helpful, both for the customer and for the ST application teams, in order to help the user while debugging the real-time software.
PTM פורסם ב: