Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Product List Associated Content
stm32 fast

The STM32 Open Development Environment is made up of four components. First is a set of Nucleo development boards that are the base motherboards containing a microcontroller. Next is a set of shield expansion boards, code-named X-NUCLEO. Each expansion board adds a functionality to the base microcontroller board. Third is a set of STM32 Cube embedded SW libraries; one for each STM32 microcontroller family, including drivers and middleware components such as graphics libraries, TCP/IP stack, file system, and USB. Finally, a set of STM32 Cube expansion Software, code named X-CUBE, which is the companion SW of each X-NUCLEO. Each X-CUBE contains all the drivers needed to run the board, with an abstract set of API.

PTM פורסם ב: