Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Product List Associated Content
fota
What is firmware upgrade Over-The-Air (FOTA)? It is the capability to upgrade the user application that is running on the wireless sensor node (on the platform’s microcontroller), transferring the new application binary image through a wireless communication channel (so Over-The-Air). In this case, the wireless communication channel is a Bluetooth Low Energy link. The ST BlueMS application embeds this capability, using a proprietary communication protocol. From the menu options the user can start the FOTA process. A file selector will be open. The user needs to look for the new application binary image that will be transferred over the air. Binary images can be stored locally (if using an Android device) or on a web/cloud-based repository (like Google Drive, Dropbox, or iCloud). The user will then select the new binary image they would like the wireless sensor node to be upgraded to and the FOTA process will start. Once the application upgrade process is completed, the user will need to reboot the device, and the newly transferred application will be running on the wireless sensor node.
PTM פורסם ב: