Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Product List
RFID Technology and Applications Slide 33

The wavelength of UHF frequencies is approximately 300 mm (12"). At these frequencies the radio waves do not pass freely through materials. In particular, moisture, water and ice cause problems by absorbing the signals. Metals also create problems with reflections. As a result of using the electric field, the ideal antenna is a dipole, as opposed to the loop favored by LF and HF transponders. This means that tags tend to be long and thin. Attempts to shorten the length of a tag usually result in reduced range. Furthermore, the performance of a tag will change depending on the material it is applied to such as a metal can, a container with liquid, or a dense material. The advantage of UHF frequencies is the ability to read a large numbers of tags in a very short time (>200 tags /second). The electric field also doesn't drop off as quickly as the magnetic field allowing extended operating ranges of greater than 5 meters. However, defining the reading zone is problematic because of reflections.

PTM פורסם ב: