Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Product List
RFID Technology and Applications Slide 4

This shows the operation of an RFID system and how a passive tag gets its energy. The three main components of an RFID system are the reader, the antenna and the tag itself. When the reader is instructed to interrogate a tag, it turns on its transmitter which sends a powerful signal to the tag. The tag then uses the RF field energy to respond to the reader's commands. All Texas Instruments' tags are passive which means there is no battery to replace or maintain. They are totally inactive until powered by the reader’s RF field.

PTM פורסם ב: