Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
OCB100-KIT Auto-Calibration Design Kit Slide 17

Before using the OPB350C125Z sensor, the phototransistor load resistance needs to be set to 2.5 Kohm by moving the shorting bar to pins 1 and 2 on the board header. A short length of 1/8” clear tubing is included in the OCB100-KIT. Snap the tubing into the optical path of the OPB350C125Z, calibrate the sensor, and test with water. The blue LED on the board will light when water is present in the optical path. If a dark fluid is inserted into the tube, the green LED will light. The sensor will also indicated bubbles in the fluid by turning both LEDs off.

PTM פורסם ב: