Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
OCB100-KIT Auto-Calibration Design Kit Slide 9

As with all optical devices, the switching condition is consistent with the phototransistor receiving a preset light level. The switching point and light level depends on several possible factors such as: ambient light variation, LED and phototransistor pair degradation, contamination of the LED or phototransistor optical path, system power variation and ambient temperature changes. These variations are reduced or eliminated by a periodic recalibration of the board.

PTM פורסם ב: