Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Product List
OCB100-KIT Auto-Calibration Design Kit Slide 4

The center biasing calibration circuit is activated by momentarily grounding pin 4. It then begins ramping current through the sensor LED from 0 mA up to 14 mA until the voltage drop across the load resistor equals 1/2 Vcc. When this point is reached, the LED current is held by the micro controller and a green calibration light blinks 3 times to indicate a successful biasing.

PTM פורסם ב: