Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Product List
Use Case System Application Dimensioning/Weighing System Alliance's Single Pair Etherrnet Use Cases

This slide shows another use case coming from the sensor industry. Shown here is a modern intralogistic dimensioning and weighing station that has barcode readers, cameras, user terminals, and detection sensors. With the help of 10 Mb single pair Ethernet including power over data line, the sensor-to-sensor communication, the sensor to the local system communication, and the sensor to remote diagnostic maintenance system can easily be optimized. I/O applications require a gateway to the Ethernet network. With single pair Ethernet, these components can be installed in an Ethernet network without using any gateways. This also provides the possibility of miniaturized interfaces that transmit high-speed data and power at the same time so small intelligent sensors can be delivered with data and power via one miniaturized interface. There are many more applications for single pair Ethernet.

PTM פורסם ב: