Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
AS5601 Slide 13

There are different tools available for the evaluation and set-up. For the first steps with the AS5601 only a adapter board is needed. A reference magnet is shipped with the board. The evaluation kit combines everything that is required for readout, configuration, and programming in a lab environment. It includes an USB I and P box, adapter board, and a magnet holder for the first evaluation. In addition, a reference module is available which can be used to replace a conventional potentiometer.

PTM פורסם ב: