Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Product List
AS5601 Slide 7

The AS5601 has an internal LDO, and can therefore be used with 5 V supply or 3.3 V supply. The output update rate and power consumption is given by the selected power mode. In the fastest mode, the current consumption is 6.5 mA and goes down to 1.5 mA at a 100 ms polling time. In addition, there is a feature called watchdog that can be used to automatically switch to the lowest power consumption if there is no activity for one minute.

PTM פורסם ב: