Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
SiC-Schottky-Slide13

The following circuit diagram shows a simplified AC/DC SMPS front end with active PFC boost converter. The purpose of the active PFC converter is to force the input current (blue waveform in the graph) to be in phase and the same wave shape as the AC input voltage (red waveform in the graph). This is achieved through the use of controller chips running advanced algorithms. The switching element Q1 is driven to provide the required load current while drawing power in correct Power Factor from the grid.

PTM פורסם ב: