Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Product List
SiC-Schottky-Slide23

Based on PFC output power and secondary repetitive peak current value, designers can select the best SiC Schottky diode rating. The rule of thumb is 1A per 100–150W of PFC circuit output power. For example: a 500W output PFC boost convert with a repetitive peak current value of 16A, would require the CSD04060 (4A, 600V) SiC Schottky diode. Note that this rating will be significantly lower than the associated silicon device. Cost/performance comparisons to silicon devices will never be one-to-one on amperage rating.

PTM פורסם ב: