Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
Film-Cap-Slide2
The typical internal structure of a film capacitor is shown in the top right diagram. The dielectric consists of two strips of metallized plastic on top of each other and rolled together. The electrode is an ultra-thin vacuum metallization layer over the plastic film. EPCOS is currently using different metallization profiles to provide different electrical parameters. Each face of the winding element is then metal sprayed, creating a conductive soldering surface.
PTM פורסם ב: