Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
Film-Cap-Slide7
This is the typical block diagram of a three-phase AC/AC converter to supply controlled power to a motor. The capacitors used in every main stage are highlighted. A star connection for the EMC filter is typical. The main purpose is to filter interferences coming from and to the grid. The DC-Link block is for smoothing and energy storage. The output IGBTs typically require snubber capacitors to protect the semiconductor from over-voltages provoked by the fast switching. The output filter will minimize the interferences generated by the IGBT module in order to provide the proper load current and voltage.
PTM פורסם ב: