Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Product List
PoE-Slide8

The graph on the left of this slide shows how much input current is needed to signal different power classification levels to the PSE. The table on the right also illustrates the maximum PD power levels required at the input of the PD, asserted classification load current for the PSE, and the associated external classification resistor used by the LTC4265 “.at ” compliant PD controller.

PTM פורסם ב: