Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
Design-Slide20

The SMDJ58CA can be considered for even higher surge resistibility protection in this application. The fuse may not be needed if the data lines are fused. However, adding these fuses provides power supply protection. For the PD (Powered Device) end, the equipment must be compatible with both Mode A and Mode B powering, thus both TVS components, that are required, must also be compatible. For the PSE (Power Supply End), it defines whether it is Mode A or Mode B, so only one TVS would be needed unless it is PoE++ that uses all wire pairs for power delivery.

PTM פורסם ב: