Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Product List
Design-Slide5

The specific criteria compliance depends initially upon the expected “ship-to” location of the application. For example, telecommunication equipment being sold to a RBOC (Regional Bell Operating Company) in the USA would require NEBS compliance. This in turn requires a product to be appropriately compliant to GR-1089-Core Issue 6. China has a series of telecommunication requirements that start with YD/T, which are very similar to the ITU-T recommendations and the UL/IEC/EN 60950-1 safety standard. The IEC 61000-4-2/4/5 are also used in both South America and Europe, depending on the specific customer and the customers preference. As the application varies from “inside a building only (intra-building)” to “outside and inside (inter-building)”, so the required compliance level will change. Inter-building applications will have higher surge resistibility levels, while antenna mounted equipment will have even higher surge level resistibility levels.

PTM פורסם ב: