Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
Conducted Emission (0.15 MHz to 108 MHz) Image of Murata's Conducted Emission 108 MHz Chart

Shown here is the block diagram of the anechoic chamber and the listed equipment used to perform the conducted emission testing. The setup and system are based on CISPR25, which is an increasingly popular benchmark and requirement for body electronics. The frequency/noise level graph on the right shows the initial test results of the board. Noise floor is represented in black and CISPR25 Class 5 specification is represented by the horizontal purple lines. The blue spectrum is the initial noise measured. As seen, the noise interval is at 400 kHz intervals, which is the same as the switching frequency of the DC/DC converter. It should also be noted that the noise level is not in compliance with CISPR25 requirements.

PTM פורסם ב:
PTM Updated on: 2023-01-10