Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
Radiated Emission (0.15 MHz to 30 MHz) Image of Murata's Radiated Emission 30 MHz Chart

Illustrated here is the measurement system that was used to test the radiated emissions from 0.15 to 30 MHz. The system is based on CISPR25. The frequency-noise level graph on the right shows the initial test results of the DC/DC converter board. Noise floor is represented in black, and the CISPR25 Class 5 specification is represented by the horizontal purple lines. The blue spectrum is the initial noise measured. Like the previous conducted test, the noise interval spikes are at 400 kHz, which is the same as the switching frequency of the DC/DC converter. The noise level measured is not in compliance with CISPR25 requirements.

PTM פורסם ב:
PTM Updated on: 2023-01-10