Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Product List
Result of Solution Radiated Emission (30 MHz to 300 MHz) Image of Murata's Radiated Emission Result 300 MHz Chart

Detailed here are the radiated emission results measured from 30 to 300 MHz after applying both the low pass filter and common mode choke coil. As seen, the low pass filter cannot reduce all the noise-troubling frequencies, while the common mode choke coil provides an added amount of filtering, allowing this design to satisfy CISPR 25 Class 5.

PTM פורסם ב:
PTM Updated on: 2023-01-10