Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Product List
Silicon Carbide MOSFETs Slide 5

Shown here is a data brief on the first SiC FET introduced by ST in 2015, the SCT30N120. It is a 45 A, 1200 V FET in the Hip247 package. This package is identical in form to the industry standard TO-247, but is comprised of materials capable of qualifying the part to 200°C operating temperature. It is in full production with data available on www.st.com. When driven at 20 V from gate to source, the RDSON at 25°C is only 80 mΩ. Even more remarkable is that at 125°C operation temperature, the RDSON only increases to 85 mΩ.

PTM פורסם ב: