Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Product List
Z8 Encore MC Slide 2

Here is a brief overview of our FMC family. Peripherals will be covered in more detail on the following slides. Some of the characteristics of the FMC family include: 4 to 16KB of flash, 512B of RAM, a dedicated 12-bit 3 phase PWM module, built-in op-amp with external gain settings, comparator that is tied to PWM module for fast shutdown, fast 2.5uS ADC, many communication engines, fault shutdown inputs, a general purpose 16-bit timer, single pin debug interface, 32 pin QFP or 5x5mm2 QFN.

PTM פורסם ב: