Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Product List
Z8 Encore MC Slide 42

The secret to a good motor control microcontroller, is not having the individual peripherals on board, but tying the peripherals together in such a way that they control the motor operation automatically. For example, the FMC16100 PWM module provides the signals to drive the power stage based upon one timer setting. Then the ADC samples the back EMF based on interrupts from the general purpose timer and samples the motor current based upon an automatic interrupt from the PWM module. The built-in op-amp amplifies and offsets the motor current sense waveform then feeds directly to the ADC. The on-board comparator monitors the motor current for cycle-by-cycle current limiting, which ties directly to the PWM module if an over load condition happens.

PTM פורסם ב: