Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
clipKIT-Slide15

Extensive CFD analysis and experimental tests have been performed to study the thermal impact of the frame-clip and spring clip in both clipKIT™ maxiGRIP™ and superGRIP™ assemblies. These studies have shown that the low profile of the frame clip and the minimal cross-sectional area of the spring clip allow for maximum airflow through the heat sink and hence maximum cooling power.

PTM פורסם ב: