Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Product List
clipKIT-Slide7

To install a maxiGRIP™ assembly using the toolset, first place a frame clip into the pocket of the base plate. Next, position the pick-and-place knob tool over the frame clip. The vertical tube in the baseplate will guide the knob to ensure the correct positioning. Then, rotate the knob tool 45° clockwise, opening the clip and locking it to the knob. Lift the two away and place them over the component, rotating them 45° counter-clockwise to release the frame clip. Lift the knob tool away, leaving the frame clip securely attached to the component.

PTM פורסם ב: