Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Product List
OpAmp-Slide10

Analog Devices has developed a novel, patented trimming process that delivers the required accuracy and performance at a very low cost. The DigiTrim™ technique allows production of precision CMOS amplifiers at costs up to 30% lower than competing solutions and with higher accuracy. This technique also allows digital control of resistor values for current matching which can bring offset voltage values under 500μV over the full common mode input voltage range (AD8602 specifically).

PTM פורסם ב: